Part Number: CC1310
Other Parts Discussed in Thread: CC1350,
Tool/software: Code Composer Studio
Hello to all,
I bought an E70-433T14S2 and I want to program it using the XDS110 which is on LAUNCHXL-CC1350-4.
I connected the Jtag pins TCK and TMS between the E70 and the XDS110 pinouts but the program doesn't load and it says:
Error connecting to the target:
(Error -241 @ 0x0)
A router subpath could not be accessed.
A security error has probably occurred.
Make sure your device is unlocked.
(Emulation package 8.0.903.6)
Can anyone help?
Thank you in advance.