This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1120: CC1120 vs CC1101 range with 0dB antenna

Part Number: CC1120
Other Parts Discussed in Thread: CC1101, , CC1190

Hello

If the output power of the CC1120 and CC1101 is compared the CC1120 has more output power +/- 6dBm. What will the approximate distance be of the CC1120 and the CC1101 with a 0dB antenna? With the assuption of minimum loss over the PCB design. What is the approximate distance a CC1190 will add? 

Thank you