Other Parts Discussed in Thread: BOOSTXL-SHARP128, , LAUNCHXL-CC1312R1, SIMPLELINK-CC13X2-26X2-SDK
Tool/software: TI-RTOS
Hey,
I have two LAUNCHXL-CC1352R1 each with BOOSTXL-SHARP128 booster-pack.
When I try to run the 15.4 Collector and Sensor examples, everything works as aspected, but I can't see anything on the LCD.
Even if I define BOARD_DISPLAY_USE_UART to "0" and BOARD_DISPLAY_USE_LCD to "1" in CC1352R1_LAUCHXL.c, the outputs in both examples still appear on the UART.
How to enable LCD Boosterpack for 15.4 example applications?
Thank you for your help!