Hi,
I understand for factory reset - i.e. switch to booting into factory image, away from say OAD image. I could press and hold left/ button2 (DIO15) at reset time on launchpad (1352R).
Couple of questions related to this:
1) Is it possible to use different input pin (instead of DIO15) for this purpose? I recall reading about backdoor pin selection, not sure if that's what I need?
2) Is the a way to use other method/s - such as, by reading certain memory location in external (area reserved in OAD) flash perhaps?
Idea/ expectation would be - by reading this location user can determine which image - i.e. factory default or one of the OAD images already in external flash to load/ run...
Thanks for your attention and help.