This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 operational description document for FCC application

Part Number: CC1310

Hi TI, 

Due to we are applying for FCC certification and the lab have a request of CC1310 operational description document, does TI have the related document?

Thanks !

  • Hi,

    This is the description we use when we certified our LaunchPad:

    ""
    Technical Description
    The LAUCHXL-CC1310 is a development tool for low power wireless connectivity solutions in the 868 MHz ISM band. The CC1310 is a System-on-Chip solution targeting long range, low power connectivity solutions.

    The LAUNCHXL-CC1310 board is equipped with a broad band Sub-1 GHz PCB antenna. The board contains a debugger to access the on-chip microcontroller debug interface for development. It exposes a USB interface that allows PC programs like SmartRF Studio to access the on-chip functionality of the CC1310 System on Chip. The board does not have any form of housing or cover. The LAUNCHXL-CC1310 is an engineering development board and cannot be used in an end product.

    The wireless control protocol is based on a 50 kbps, 2-GFSK modulation @ 10 dBm. SmartRF Studio 7 is used to set the CC1310 into this mode in either RX or TX to exercise the device.

    The CC1310 System on Chip has a differential RF output. On the LAUNCHXL-CC1310 this differential output is fed to a discrete balun and a filter towards a pcb antenna.
    ""

    You can use this as a baseline for you own CC1310 product.

    -Simon