1. CC1125在接收按DMR标准ETSI TS 102 361-1定义的信号时接收灵敏度偏低,大约在-108dBm左右。这是不是由于CC1125接收端缺少与发射端相对应的“根升余弦”滤波器导致的?如果是,有什么办法解决?如果不是,有可能是什么原因导致的?
2. 根据用户手册描述,接收端设置的频差应与发射端信号频差保持一致。经测试,发射端信号频差与接收端寄存器(DEVIATION_M,MODCFG_DEV_E)设置不一致(相差大于0.4kHz)时接收灵敏度急剧降低。CC1125有没有相应的方法使得接收端可以在信道滤波器带宽内自动追踪发射端的发射信号频差
3. 根据用户手册描述,使用CC1125的FeedBack to PLL(配置FREQOFF_CFG寄存器)功能可以提升接收灵敏度,但是经过测试所有可能的寄存器值发现,开启FeedBack to PLL性能最好的情况下(FREQOFF_CFG寄存器设置为0x38)也没有关闭FeedBack to PLL(FREQOFF_CFG寄存器设置为0x20)的接收灵敏度高,这是为什么?