This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: Support for High Speed modes in CC1352P

Part Number: CC1352P
Other Parts Discussed in Thread: CC1310, CC2650,

Previous parts in the CC26xx and CC13xx ranges (CC2640R2, CC2650, CC1310) have supported high speed transfer modes up to 4Mbps, sub 1GHz and 5MBps, 2.4GHz albeit some of the details are obscure and may require NDA to fully implement.

Are cross-compatible High Speed modes possible in the CC1352P which can interoperate with appropriate CC26xx parts at 2.4GHz or with CC13xx at 900MHz? or in any other of TI's dual-band parts?
If not, is there any plan to implement them in future?