This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: CC1200

Part Number: CC1200


Dear Ladies and Gentlemen,

we would like to measure the temperature with in-built feature of CC1200.

According to application note (SWRA415D) the analog voltage can be output on GPIO1 pin.

As this pin is also used for SPI transfer, we would like to measure the voltage on different GPIO pin.

Is it possible to set that analog voltage measuring temperature with GPIO0_ATRAN,..  GPIO3_ATRAN to different pin?

What are GPIO0_ATRAN for?

What are GPIO2_ATRAN for?

What are GPIO3_ATRAN for?

Is the measurement during RX and TX of IC possible?

Best Regards Stefan