This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: abou cc1310 Transmit carrier mode

Part Number: CC1310

  

we  want use  CC1310  Transmit carrier mode,  use   below  code can send  carrier, but what  cmd can be stop?  we use  "  RF_cancelCmd(rfHandle, result, 0);"  in other  task  , can not stop.

   RF_Params rfParams;

    RF_Params_init(&rfParams);

 

    /* Explicitly configure CW (1) or Modulated (0). Default modulated mode is PRBS-15. */

    RF_cmdTxTest.config.bUseCw = 1;

 

    /* In order to achieve +14dBm output power, make sure .txPower = 0xa73f, and

    that the define CCFG_FORCE_VDDR_HH = 0x1 in ccfg.c */

 

    /* Request access to the radio */

    rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);

 

    /* Send CMD_FS and wait until it has completed */

    RF_runCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);

 

    /* Send CMD_TX_TEST which sends forever */

    RF_runCmd(rfHandle, (RF_Op*)&RF_cmdTxTest, RF_PriorityNormal, NULL, 0);