Other Parts Discussed in Thread: CC1310, SYSBIOS
Tool/software: TI-RTOS
HI i think i have been having problem with SCS and RF
this problem i skip before
My case was follow , i am running a LC Sensor Controller program .
I was
and tios
the value of the 3LC is here as show
2) i try to out the SCS into the empty.c with uart from the resource explorer. the result was
show as below
the result was consistent .
3. Finally i intergate it with the RfPacktet.TX . (ps i run with standalone Rfpacket TX and RX and it works )
the code i attached in below,
the value of the LC sensor (LC value in program was come out mistake)
MY question:
1. Can someone help me to solve the problem of case all the LC value was all go wrong when it come with the TX program.
2.in the program , i try to comment out the
/* Request access to the radio */
rfHandle = RF_open(&rfObject, &RF_prop, (RF_RadioSetup*)&RF_cmdPropRadioDivSetup, &rfParams);
/* Set the frequency */
RF_postCmd(rfHandle, (RF_Op*)&RF_cmdFs, RF_PriorityNormal, NULL, 0);
and the result come to normal to the emtpy.c one
3. Is it possibile that i only trigger the TX at some time or some interrrupt?
4. will the possible casue of error was the stack, as my LC program was run all the way time and so do the TX part.
Thanks
Jeff