This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352R: Interfacing with TI-15.4 coprocessor via SPI

Part Number: CC1352R

Hi,

Referring to this year-old thread - e2e.ti.com/support/wireless-connectivity/sub-1-ghz/f/156/t/683426 
I understand SPI was Not supported for interface with TI-15.4 CoP - curious if that's changed since?
Or is it in the works perhaps(?) - planned for release in the upcoming CC13xx/ Linux SDK versions?

Please advise. Thanks.

Best,
SE

  • Hello SmartEng,

    No, it is still the same. You can go ahead and add SPI to the Co-Processor example and it should work. But as the thread suggest we cannot guarantee that it will 100% work since we have not run it through our tests in house.

    Regards,

    AB