Hello,
We are planning to use 32kHz clock out for other devices. In CC1312R datasheet it is mentioned that "When using a crystal or the internal RC oscillator, the device can output the 32 kHz SCLK_LF signal to
other devices, thereby reducing the overall system cost".But in datasheet it is not mentioned which pin we can configure as 32 kHz clock out. Is there any specific pin or can any GPIO be configured for the same ?