This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Recommend a high data rate modulation device

Part Number: CC1310
Other Parts Discussed in Thread: CC2640

Hi,

1. Pulse edge should be within 2us. It's very important to make operation in time. So we search high data rate device.

2. Either Sub1G or 2.4G is fine, but must be >800MHz.

3. Not used for wireless communication, transmit a 5ms on/off signal through cable by use of the device modulation function.

The highest datarate of CC1310 is 4Mbps on 915Mhz. CC2640 is 2MHz. Is it right?