This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352P1 433MHz Sniffer support.

Other Parts Discussed in Thread: LAUNCHXL-CC1352P1

Hi, I'd like to know how the channels of the 433MHz band are determined or calculated while using the LAUNCHXL-CC1352P1.

I was using the Smart RF Sniffer Agent v1.7.0 and noticed that the "IEEE 802.15.4g - GFSK 50Kbps - 433 MHz" is using a default 0.2 channel spacing and the central frequency for channel 0 is 433.3 MHz.

I could not find any references for this configuration on the IEEE 802.15.4-2015 specification.

Are there any documents you can recommend, or is this something that Texas Instruments has determined on their own?

Maybe it has to do with best performance and measurements like that. I would really like to know.

Thank you.