This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC85XXDK-HEADSET-RD: Trouble running packet error test with Purepath Wireless Commander

Part Number: CC85XXDK-HEADSET-RD
Other Parts Discussed in Thread: CC8530, CC8531

I'm trying to get the packet error test running with two CC85XXDK-HEADSET-RD evaluation boards. I'm using Purepath Wireless Commander (V1.0.0, build 36940) to run the stock PER test (prod_test_per_auto.ppwptc). Each of the evaluation boards is connected to a CC debugger, called TESTER and DUT. However, every time I run the PER test, none of the tests pass.

The evaluation boards are placed directly beside each other, so in theory the packet loss should be extremely low. Am I doing something wrong here?

Here is a screenshot of Purepath Commander after it tries to run the PER test.

I do have a proprietary design using the CC8530. The design is based off the evaluation board, and eventually I'll have to get this test running on it.