This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P: I used CC1352, and now I use an external ADC (ads131a04) to sample, but the data speed is only 5kbps.

Part Number: CC1352P
Other Parts Discussed in Thread: ADS131A04,

Hi,

     I used CC1352, and now I use an external ADC (ads131a04) to sample, but the data speed is only 5kbps by SPI.

    The problem is that when reading ADC data through the SPI port, the speed can only reach 5kbps and cannot reach 25.6k as stated in the manual. Could you help me?

   If i use CC1352 internal ADC, the data speed can be read at a rate of 25.6k.

Lemon