This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352R1: Reset both cores with OpenOCD

Part Number: LAUNCHXL-CC1352R1

Hi,

I'm working on project for this part in VS Code and flash/debug using OpenOCD.

I've noticed on the OpenOCD output the following message:

Warn : Only resetting the Cortex-M core, use a reset-init event handler to reset any peripherals or configure hardware srst support.

Which seems to be accurate because after that, some calls to the radio API hang. From what I understood from the part manual this is caused by the radio core being in a unknow state. If I manually reset the board and after that start the debug, those hangs do not happen. This is consistent with the explanation and makes sense.

Now, if I use Code Composer to flash and start debug of one of the sample projects, it launches the debugger just fine. No need to manually reset the board.

I did notice on the CCS output the following message:

Cortex_M4_0: GEL Output: Board Reset Complete.

This leads me to think that the OpenOCD configuration files for the CC13x2/26xx are missing _that_ board reset.

Can you please confirm the above, what could be missing and/or any extra arguments that should be added to the command line launching OpenOCD?

Thanks!

  • "Board Reset" is the term CCS uses for a reset done by asserting the nSRST pin of the JTAG header. (It's not called System Reset because the name already had a couple other uses, either the reset done via the ICEPick JTAG router hardware or the Cortex M system reset via the AIRCR).

    What version of OpenOCD are you using?  It looks like the version you're using is defaulting to using the vector reset to reset the Cortex M core. To do the equivalent of the board reset, you would need to use the nSRST pin.  The following could be added to the target config file:

    reset_config srst_only
    adapter_nsrst_delay 100

    However, the last official release of OpenOCD (0.10.0) has a bug in the reset handling, and this won't work for the CC13xx/CC26xx targets.  (It pulls the reset once, re-runs the code needed to enable JTAG, then pulls reset again leaving the target in an undebuggable state.)

    We have a work around in a copy of OpenOCD we maintain at https://git.ti.com/sdo-emu/openocd. And in this version, we're using nSRST reset for these targets.

  • thank you so much for the detailed explanations!

    I'm indeed using the official 0.10.0 version of OpenOCD.

    I'll switch to TI tweaked version as suggested.

  • I've managed to build the TI OpenOCD in Windows and I'm now using it.

    The initial error is gone but I now have this on the OpenOCD output:

    openocd: Info : JTAG tap: cc13x2.jrc tap/device found: 0x3bb4102f (mfg: 0x017 (Texas Instruments), part: 0xbb41, ver: 0x3)
    openocd: Info : JTAG tap: cc13x2.cpu enabled
    openocd: Error: Debug regions are unpowered, an unexpected reset might have happened
    openocd: Error: JTAG-DP STICKY ERROR
    openocd: Error: Could not find MEM-AP to control the core
    openocd: target halted due to debug-request, current mode: Thread
    openocd: xPSR: 0x61000000 pc: 0x1000118e msp: 0x11001ff0

    I have to say that I can run the debug fine, so not sure if it's completely safe to ignore those. Just wanted to check it with you.

    Thanks,