Other Parts Discussed in Thread: CC-ANTENNA-DK2,
Hello,
I have tested the FR01-S4-224 antenna from your CC-ANTENNA-DK2 dev. kit for 2.4GHz and 868MHz and would like to use it in my design. However, I don't have equipment to do the antenna tuning at the moment and thus would like to follow the most optimal design guidelines. Up until now I was following the LAUNCHXL-CC1352P1 design (for 20dBm boost of the 868MHz), however after the RF switch part I wanted to use the tuning which is presented in CC-ANTENNA-DK2 dev kit (Board Design #3). The problem is that it differs from the one presented in the FR01-S4-224 user manual. So, which one should I follow for the same Layer stack as in LAUNCHXL-CC1352P1?
Some side verification questions:
- Do you have a reference design for the CC1352P1 with the IPC Balun instead of discrete matching network? Would you suggest using an IPC balun instead of discrete components?
- I know it has been asked before about Atliums pcb files of the CC-ANTENNA-DK2, do you have any other format which could be converted to Atlium pcb files, e.g. .ALG files?
Kind Regards,
Den