Other Parts Discussed in Thread: CC1310
Tool/software: Code Composer Studio
Hi Team,
I wanted the board to work on 868MHz, so configured as follows,
/*! Setting for Phy ID */
#define CONFIG_PHY_ID (APIMAC_GENERIC_ETSI_LRM_863_PHY_131)
in the config.h file. The board does not work with this configuration. In the sense, it nodes do not connect to the network.
The board works fine when configured to 915MHz.
I believe the board is optimized for 915MHz.
So, to work with 868MHz with the same board what is that I need to do, and could you please let me know the procedure for extending the range of it.
Thanks in advance.
Regards,
Shubha