This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1125: Emissions code for FCC approval

Part Number: CC1125

Hi Team,

Our customer is applying for FCC approval and it states that they have to enter an emission code for CC1125.

Can you share with us the emission codes for CC1125?

If there would be needed actions to be done to obtain the designators, please let me know.

Thanks in advance.


-Jejomar

  • Hi,

    FCC Certification is required for a product Not for a Chip. So, we don't have any emission code for the chip itself.

    CC1125 is suitable to use in the following Regulations.

    Suitable for systems targeting compliance with:

    Europe: ETSI EN 300 220 category 1, ETSI EN 54-25, ETSI EN 300 113, and EN 301 166

    US: FCC CFR47 Part 15, 24, 90, 101

    Japan: ARIB RCR STD-T30, T-67, T-108

    They can contact their Certification Lab for the advice on how to get the certification?

    Thanks,

    PM