Hello,
We design the custom board using CC1310F128 5x5 chip for our project and our project is working ok
The antenna on our custom board is PCB helical antenna.
The communication between our two custom board is working ok
Now we need to add one more device into our network. but because of size restriction, we cannot design PCB helical antenna on our new device, so we decided to add 868 MHz chip antenna instead of the PCB antenna on our design. so my query is
- does chip antenna communicate with PCB helical antenna
- do we need to consider any design parameters while designing custom board with chip antenna so it communicates with PCB helical antenna
- does chip antenna effect on communication range