Hi Champs,
Our customer has recently purchased CC1200DK and has facing a problem.
Symptoms are as follows:
One of the SmartRF Transceiver Evaluation Board does not work in SmartRF Mode.
A PC does not recognize it though USB.
After an USB mode switch S1 on the board is changed from SmartRF Mode to UART mode, PC detects USB and the display on the board works fine.
With SmartRF Mode, LED D6(USB LED) ,which indicates USB operation, is ON.
Even though a daughter board is removed, LED is kept ON.
I believe that normally the LED is blinking (100msON-900msOFF) and No RF-IC is detected.
Let us clarify if there are nay check points.
Thank you so much for your kind support.
Best regards,
Hitoshi