Hi,
My customer has a question about CC1310 and also looking at results in terms of consumption that are behind competition ... which declares much smaller absorption.
We will have to acquire an analog signal at 100Hz and for example every 10 samples do some simple calculations and if a desired value is obtained it is necessary to activate the core of the micro Cortex M3 .. otherwise it remains in low consumption.
Currently we have tried to implement it with use of the Sensor Controller as suggested also by swra578 pag.17 (around 19uA) .... I wonder though if this is the technique with lower consumption.
I also ask you if CC1310 can still be considered the optimal choice for a new development.
On the CC1312 consumption performance has been improved as far as I know.
So which are the best way to obtain the least consumption?
Many Thanks,
Antonio