In this schematic at the top left where it says 'Mount 0R resistor: C14' did they mean R3?
Also if I don't use 'Option A' do I just not put those components and that's it or do I connect L2 to C25, not sure of this because on the board layout L2 and C25 are far apart I would have to put a wire.
SCHEMATIC - CC1120 Skyworks 30 dBm 169 MHz Ref Design Rev1_0_2.pdf