Hi team,
I am using CC1101 at ~410MHz.
Some modules have very high current consumption: 700mA @3.4V. The transceiver is very hot. However, all the Tx Rx activities are still okay.
I tried to reset the MCU to re-initialize the transceiver but it doesn't help. Only power cycle can help. It happen to some specific module and the issue moved with the ICs when I tried to solder them on another board.
The erratasheet doesn't mentioned any large current consumption.
Please advise what I should further check.