hi,
we are considering CC1310 for a new designs (BA, alarm systems).
On the old radio we used these RF characteristics:
- Frequency: 866.09838 MHz
- Modulation: 2GFSK
- Data rate: 76.767 kbps
- Deviation: 31.738 kHz
but we are facing some challenges in setting the same parameters with the SmartRF studio (the deviation always goes back to 31.500 kHz, it looks that tool has some auto calculated boundaries which we can't go beyond):
Any help is more than welcome.
Thanks a lot in advance
KR
Vincenzo