The CC1120 IC's SO pin shows no response on 4 wire spi interface with mcu. I tried to write data in the registers and read it on the SO pin to check if the ic is working properly, but no data was read. Even on pulling the CSn low, there is no change in the level of SO, it does not go low.
On testing the code on the cc1120 module, it works fine, but does not work with our design board.
Can anyone elaborate why is this issue occurring?
Is there any specific way in which this package needs to be soldered by hand?
Also, is there any way in which we can check whether the IC is working properly?
I have attached the KICAD board file and schematic, along with the reference schematic.
Thanks and regards,