Hi,
there seem to be a few different frequency bands that could be used in China for short range device. Most common are the 433MHz band and 779MHz to 787MHz band (if I am reading the standard correctly). We have a design based on the CC1312 already for the US and EU that we want to now adapt to the Chinese market. The device description on the home page states "Flexible Sub-1 GHz radio supporting industry standard frequency bands (315 MHz, 433 MHz, 868 MHz, 900 MHz, and more) to meet the industrial needs" but in the datasheet I see no reference to the lower frequency bands.
Q1) Can we use the CC1312r for the Chinese market?
Q2) If yes, have you done any testing towards the Chinese requirements?
Q3) Which of the frequency bands do you recommend for China in that case?
Best Regards
Peter