Part Number: CC1350STK
Other Parts Discussed in Thread: CC1350, UNIFLASH,
Dear Experts Team,
When i am trying to convert the CC1350 device from a BLE device into sub-1GHz device in the initial step of pre-work.
""Rev 1.4.5 of the CC1350 SensorTag contains a pre-production factory image, an update is needed in order to use all features on the CC1350 SensorTag. This procedure requires a debugger dev pack. Please update to the latest image by following the below steps, it is only needed to do this once.
- Remove the battery from the CC1350SensorTag.
- Connect debugger dev pack to the CC1350 SensorTag and connect it to your PC via USB.
- Click the button below in order to erase the external flash memory of the CC1350SensorTag.
NOTE: The first time you do this, a small flash utility will need to be installed locally on your PC.""
i have done the step 1 and step 2 to install local small flash utility like TI Cloud Agent bridge, etc. There are error coming out everytime after the trial as shown below:
I have tried again accordingly, even reboot computer. Would you please advise?
Thank you for kind attention.
Best Regards,
Johnny Lam