Other Parts Discussed in Thread: CC1190
Hi,
we think about using the TI-15.4 stack for a smart home application. Because we want to communicate between several floors of the customers house, we have to achieve the best possible range and building penetration.
Further, the radio system should be able to pass the ETSI EN 300-220.
After some investigations, we found two approaches which appear very promissing, for this purpose:
- TI-15.4 Long Range PHY, with Frequency Hopping
- Range Extension with CC1190 on the gateway side
While, as mentioned in ETSI 300-220, the high gain mode could only be used in a smal frequency band (869,400 MHz to 869,650 MHz), the LRM is usable over the hole SRD range (863-870 MHz). In our understanding this in opposition to eachother.
What is the better approach to achieve the best radio performance inside a building, LRM or Range Extention? Is it possible to combine this two technologies within TI-15.4 stack? For example, it would be conceivable, to do FH over the whole 868-band and activate the CC1190 just for the allowed band. Would that be a conceivable approach?
Thank you for helping and best regards
Felix