Other Parts Discussed in Thread: CC1352R, CC1310,
Tool/software: Code Composer Studio
Hi,
We are using LPSTK-CC1352R with CC1310 LaunchPad + sensor and collector examples. We would like to know if it is possible to implement the collector with LPSTK-CC1352R too, so that we can avoid having to program the CC1310 LaunchPad as collector, and only use it for UART/debugging communication instead. We tried to directly flash at CCS the CC1352R collector example to LPSTK, but the following error appears:
Cortex_M3_0: File Loader: Memory write failed: Timed out waiting for target flashloader to execute command.
Cortex_M3_0: GEL: File: ...\collector_CC1352R1_LAUNCHXL_tirtos_ccs_syscfg\Release\collector_CC1352R1_LAUNCHXL_tirtos_ccs_syscfg.out: Load failed.
Does that mean that LPSTK-CC1352R can only be programmed as a sensor (not as a collector)?
Thanks in advance,
Mario