This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1352R: Decrease power consumption using ApiMac_attribute_battLifeExt

Part Number: CC1352R

Tool/software: Code Composer Studio

Hi,
I'm looking for possible ways to decrease the power consumption of a custom sensor board. I'm using TI 802.15.4 and Non Beacon Mode.
Could the parameter ApiMac_attribute_battLifeExt help me on this?
If yes, how does it work, and how could I use it?
 Thanks for your attention,
  • Hey Bruno,

    Unfortunately the parameter is only used in Beacon enabled networks and is not used for Non Beacon Mode.

    As a reference, here's a link to a document with design considerations for our low power mcu's: http://www.ti.com.cn/cn/lit/an/swra640c/swra640c.pdf .  I hope you've seen this already, if not, I highly recommend going through it.

    What are your requirements in your application? You may be able to save more power in certain modes depending on your requirements. One way to reduce power consumption is to reduce your reporting/polling interval and lower your packet size so that the radio is on for the least amount of time possible.

  • Thanks for your answer, Ammar

    I had already read this pdf, it is really useful. I was just checking the firmware parameters to see whether there were things I could improve concerning low power.

    Thank you again,

    Bruno