This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2510 don't wake from PM1 mode from timer or external interrupt

Other Parts Discussed in Thread: CC2510

Hi,

I have 2 devices of cc2510 which are running almost a week (without reset) and running the same program:

They are going to sleep for 3 seconds in PM1 mode and wakes from the timer . (it can be waken also from external interrupt), after they wake up, they check the status of their battery and status of some ports and goes to sleep.

Yesterday I found the devices are not working, it seems like they went to sleep forever and don't waked up (not from the timer and not from an external interrupt),

only reset return the devices to their work.

After reset one of the devices is working properly.  But the second device, after a while, went  to sleep forever again (the same problem again) .

 

What can be the problem?

 

Thank you very much for the help,

Elena.