Tool/software: Code Composer Studio
Hi all,
we try to add period timer into our application. We test "timerLed" project. The current is 0.9mA when start timer. Can we decrease this current? Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi all,
we try to add period timer into our application. We test "timerLed" project. The current is 0.9mA when start timer. Can we decrease this current? Thank you.
Hi Kimi
A current consumption of 0.9 mA for that example is as expected. The device will be in Idle mode when the Timer is on, consuming 590 uA. the peripheral power domain consumes 82.3 uA and the timer, 67.8 uA (when IDLE). this adds up to 740 uA. In the exampl, the timer is running, and the current consumption is around 850 - 900 uA (I measure 860 uA).
BR
Siri