This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: Frequency change related questions

Part Number: CC1312R


Hi 

I am working on a proprietary FHSS protocol so I need to change Rf frequency frequently (aproximatly every 20ms) and I have several questions:

1) If I am not goin to change the rf band (lets say that I am working in 868MHz band) does it have to always change frequency settings in both RF_cmdPropRadioDivSetup (rf setup) and RF_cmdFs, or in case that not changing rf band the change with RF_cmdFs is enought?

2) Are there any "rules" how big could be the difference betwee both frequences set with DivSetup and cmdFs?  

3) Is there a faster approach to change rf setup parameters runtime than "change Setup"->RF_control->RF_yield? I mean is there a way to avoid losing time for RF_yield (real rf core power-off).

Regards

Dimitar