If I have two cc1350 boards communicating with each others using subghz at 868 freq band and another two boards communicating with each others using subghz at 868 freq band, find the questions below:
1. Can I prevent the interference in the data sent and received in the two different subghz networks while using the same frequency band?
2. Is there a minimum distance that should be between the two different networks to prevent the interference of the data in both networks?