Other Parts Discussed in Thread: CC1350
Tool/software: TI C/C++ Compiler
Hi,
I am using CC1350 Launchpad powered through XDS110(type AB micro cable). I have loaded the pinStandby Simple Link CC13x0 SDK example code.
I am measuring the Current by connecting a 100ohm resistor across Vsense and getting the voltage as 100mV, which means the current is 1mA, which is too much during the standby mode.
I cannot see any change in the current after the standbyDuration as seen in the DSO.
In some examples i noticed i should disable the sensor tags, since i've not used any sensor, I think there is no issue coz of the sensors.