Hi,
I setup the ti demo to use FH using ti154stack_linux_x64_2_08_00_04, simplelink_cc13x2_sdk_2_30_00_45 for the CoP and Sensor since these are rev C boards. Everything connects and talk to each other but is there a way to reduce the time it takes to re-join the network? The PCS_event was triggered after 3 seconds here but often it takes 6 seconds. Then it takes another 16 seconds to trigger the association event. Is this normal?
[2020-06-12 13:23:26.578] TI Sensor
[2020-06-12 13:23:26.580]
[2020-06-12 13:23:26.580] sensor start evt
[2020-06-12 13:23:26.580]
[2020-06-12 13:23:26.580] rejoining
[2020-06-12 13:23:26.583]
[2020-06-12 13:23:26.583] State Changed: 2
[2020-06-12 13:23:26.587]
[2020-06-12 13:23:29.842] PCS_EVT
[2020-06-12 13:23:29.842]
[2020-06-12 13:23:45.733] ASSO_REQ_EVT
[2020-06-12 13:23:45.736]
[2020-06-12 13:23:46.720] association confirmed
[2020-06-12 13:23:46.725]
[2020-06-12 13:23:46.725] ssf_networkupdate
[2020-06-12 13:23:46.725]
[2020-06-12 13:23:46.725] Device Restarted
[2020-06-12 13:23:46.725]
[2020-06-12 13:23:46.725] Frequency Hopping
[2020-06-12 13:23:46.725]
[2020-06-12 13:23:46.725] State Changed: 4
Thanks,
Walter