Other Parts Discussed in Thread: CC1310, CC2650
I have a custom-made sblAppEx for CC1310 using the same header file than the TI project. I have upgraded my board to CC1312R so I'm adapting everything.
#define SBL_MAX_DEVICES 20
#define SBL_DEFAULT_RETRY_COUNT 1
#define SBL_DEFAULT_READ_TIMEOUT 100 // in ms
#define SBL_DEFAULT_WRITE_TIMEOUT 200 // in ms
#define SBL_CC2650_PAGE_ERASE_SIZE 4096
#define SBL_CC2650_FLASH_START_ADDRESS 0x00000000
#define SBL_CC2650_RAM_START_ADDRESS 0x20000000
#define SBL_CC2650_ACCESS_WIDTH_32B 1
#define SBL_CC2650_ACCESS_WIDTH_8B 0
#define SBL_CC2650_PAGE_ERASE_TIME_MS 20
#define SBL_CC2650_MAX_BYTES_PER_TRANSFER 252
#define SBL_CC2650_MAX_MEMWRITE_BYTES 247
#define SBL_CC2650_MAX_MEMWRITE_WORDS 61
#define SBL_CC2650_MAX_MEMREAD_BYTES 253
#define SBL_CC2650_MAX_MEMREAD_WORDS 63
#define SBL_CC2650_FLASH_SIZE_CFG 0x4003002C
#define SBL_CC2650_RAM_SIZE_CFG 0x40082250
#define SBL_CC2650_BL_CONFIG_PAGE_OFFSET 0xFDB
#define SBL_CC2650_BL_CONFIG_ENABLED_BM 0xC5
#define SBL_CC2650_BL_WORK_MEMORY_START 0x20000000
#define SBL_CC2650_BL_WORK_MEMORY_END 0x2000016F
#define SBL_CC2650_BL_STACK_MEMORY_START 0x20000FC0
#define SBL_CC2650_BL_STACK_MEMORY_END 0x20000FFF
For CC1312R, everything is unchanged except:
#define SBL_CC2652_PAGE_ERASE_SIZE 8192
#define SBL_CC2652_BL_CONFIG_PAGE_OFFSET 0x1FDB
What else should I change? Am I missing anything in those defines?