What is the range for the short addresses in TI15.4 stack?
- If Max devices are configured to be 100 are the possible short address values 0 to 99? Is there any possibility that devices get some other values?
- When the device in address 10 has been missing and all other addresses are occupied, if a new device is to be added to the network, will it be given the address of 10 or another address by the collector (outside of the range 0-99) ?
- What should be done if I want the collector to forget about the missing devices and fill those addresses by the newly joined sensors?