This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352P: Need to achieve stable communication on 500-600m range

Part Number: LAUNCHXL-CC1352P
Other Parts Discussed in Thread: CC-ANTENNA-DK2,

Customer needs to achieve a stable communication on  500-600m range. Currently, with antenna #12 they are able to maintain communication with minor obstacles - trees, fences, ext only on about 100m.  Will 500m distance be achievable with higher output power, different antenna (has to be omni-directional as sensor is mounted on moving target), any software opportunities? 

  • Hi,

    Why are you using CC-Antenna-DK2 #12 ?

    The optimum choice of antenna at 868/915 MHz would be CC-Antenna-DK2 #9 as used on the LP designs.

    Are you testing the range on a LAUNCHXL-CC1352P1 ?

    Frequency ?

    Data rate / PHY ?

    Output power ?

    Regards, 

       Richard