Other Parts Discussed in Thread: , , CC2652P, CC1310
Hi,
As I know, there are three versions of LAUNCHXL-CC1352P as below.
LAUNCHXL-CC1352P1: 868/915 MHz up to 20 dBm, 2.4 GHz up to 5 dBm
LAUNCHXL-CC1352P-2: 868/915 MHz up to 14 dBm, 2.4 GHz up to 20 dBm which can be used to support both CC1352P and CC2652P
LAUNCHXL-CC1352P-4: 433 MHz up to 14 dBm, 2.4 GHz up to 10 dBm
I want to design like as below, is it possible?
433MHz(470-527MHz exactly) up to 20dBm, 2.4GHz up to 5dBm
If yes, can I get the reference design files?
Thanks in advance.
Kevin