Part Number: CC1312R
Tool/software: Code Composer Studio
Hello,
I am working on CC1312 custom boards. They work fine, except for one of them, which exhibits the following problem:
If the device has already been programmed, I receive this error when I try programming it again:
Cortex_M4_0: GEL Output: Memory Map Initialization Complete. Cortex_M4_0: GEL Output: Board Reset Complete. Cortex_M4_0: Target timed out! (Block 0) Cortex_M4_0: Status 0xFFFFFFFF: Target flashloader has not returned any status. Unknown error! Cortex_M4_0: Command=20 -- addr=0x00002000 -- length=0x00002000 Cortex_M4_0: File Loader: Memory write failed: Timed out waiting for target flashloader to execute command.
I have two choices then to "fix":
1. Power cycle the device;
2. Erase flash memory
I use a LaunchPad with XDS110 two-wire JTAG to program, voltages look good. I have also tried slowing down the JTAG clock, to no avail.
Any pointers where to look and what to try are appreciated.