This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi team,
I am using C:\ti\Simplelink_audio_plugin_3_30_00_06\RTOS\CC1312R1_LAUNCHXL\easyLink\rfAudioRx.
I found that the sound quality is very poor, but using the Echo project for non-RF testing, the sound quality is very good.
I conducted an experiment and compared the data transmitted by TX with the data received by RX, and found that the higher 8 bits are the same, but the lower 8 bits are different.
Sometimes, the higher 8 bits may be different.
The data on the red line is TX data, and the data on the bottom is RX data. When I send fixed data, the data of TX and RX are the same.
Can you help to check it?
Regards,
Kevin
Hi Kevin,
Can you provide a picture of your system?
For the rest, try to keep the jumper wires as tight as possible. It would be even better if you could solder the jumper wires on the boosterpack directly.
Regards,