This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: RTOS How to wakeup using AONEventMcuWakeUpSet() for edge detect on DIO23?

Part Number: CC1310

What value should I use for the second parameter to AONEventMcuWakeUpSet(AON_EVENT_MCU_WU0, ui32EventSrc)
in order to wake up when DIO23 goes low?

Note that the constant AON_EVENT_DIO23 is NOT defined for the CC13XX.
For CC26xx, the value AON_EVENT_DIO23 appears to map to 26. I tried
setting ui32EventSrc to 26 for the CC13XX with no luck.


An example project for powering down and then waking up the CC1310 using DIO23 would be very helpful.

Note that I am using the CC1310 LaunchPad development board  with a 7-mm × 7-mm RGZ VQFN48