Hi,
I am experimenting with a few Ebyte E79 modules which contain a CC1352P with an 434MHz matching network as well as a separate 2.4GHz one. The PA outputs are matched to 434MHz and a T/R switch selects either the PA outputs or the sub-1GHz input/output ports.
It comes programmed as a wireless UART. I reprogrammed one module using CCS; programming works fine.
Using SmartRF studio settings for LAUNCHXL-CC1352P-4 I am able to transmit at a 10dBm level. I actually measure 8dBm on a spectrum analyzer, but this seems fine (some power is lost in the matching network and filter, etc).
I could not get 20dBm settings from SmartRF studio for 434MHz, so I used the settings (all the 3 overrides) for 915MHz, configured for LAUNCHXL-CC1352P-1.
In this mode, I get about 15dBm output at the antenna connector. Not bad, but there should be maybe 3dB more that are lost. I am assuming that the overrides are the cause.
Are there overrides that work well with this module for 20dBm output? If they are not available, I am willing to experiment with modified overrides, starting from the 915 ones, but I have no idea what to try to modify.
This is for an amateur radio application, in which 20dBm are allowed (actually much more) between 430 and 440MHz.
Thanks, Sivan