Other Parts Discussed in Thread: CC1190, CC1310
I am trying to test 7 FCC units, a combination of CC1310 and CC1310+CC1190 products in the 7x7 package. The units have code in them and Smart RF Studio wasn’t able to stop the firmware on the CC1310 till quite far in the Smart RF Studio boot process.
Usually as soon as I plug in the powered Launch board 2 wire program connections (RST, TMS, TCK, GND) SmartRF Studio takes control of the CC1310 and stops the code from running
I tried doing the FCC pre-testing, but while SW always seem to communicate with the target device, the commands required to turn on the transmitter are very flakey, working sometimes other times refusing to work. Basically on bad units, when the SW attempts to turn on the transmitter, the commands that appear in the command output window show up about 10 seconds later than they normally do and the unit never turns on. It seems like whatever FW is running on the CC1310 is not able to interpret the commands it is being sent?