Other Parts Discussed in Thread: CC1310, CC1352P, CC1312R, CC1352R
Hello, expert,
I'm testing with cc1352P2 development board. The project path is
C:\ti\simplelink_audio_plugin_3_30_00_06\examples\rtos\CC1352P_2_LAUNCHXL\easylink\rfAudioTx、Rx.
We found that in the case of 16K sampling rate, there will not be the phenomenon in the attachment. When the sampling rate is 24K, 32K and 48K, the phenomenon in the attachment will appear.What should we do to solve this problem?Is it related to the clock allocation of codec chip?
Phenomenon description: after the audio transmitted by RF is normally played for a period of time, there will be a small noise suddenly, and then the noise will gradually increase, and it will suddenly return to normal after a period of time. Then it slowly becomes noisy, alternating between normal and abnormal.