Dear Sir,
We are using CC1312R in our project. what i found is below.
When it goes to ideal task, it checks if power policy is enabled. If power policy is enabled then it will go to idle mode. When i checked the power constraints, they are set to 6 which means that the standby mode and shutdown modes are not allowed. So i manually allowed the standby mode. When it goes to PowerCC26XX_standbyPolicy(), it loads the ticks with next schedule wakeup. when print the tick value, it is 7 and time will be 70uS. Which is very less.
How can i make the chip to stay in standby mode for longer period of time?
Later, i need to implement it to stay in standby mode between beacon periods. Can you please guide me what are the steps to implement that?
Thank you.
Satyakam.