This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1310: Cc1310 program reset function sometimes fails

Part Number: CC1310

Tool/software: Code Composer Studio

Hi

Recently, we encountered a problem in the development of cc1310 oad. When downloading the new firmware, calling the reset function to reset the program does not work. Sometimes, the program will be completely stuck in this place. We have tried many kinds of reset, such as software reset and watchdog reset.

We have used the following functions

1, #define HAL_SYSTEM_RESET()  (HWREG( AON_SYSCTL_BASE + AON_SYSCTL_O_RESETCTL ) |= AON_SYSCTL_RESETCTL_SYSRESET_M);

2,  SysCtrlSystemReset();

3, Watchdog_open(Board_WATCHDOG0, &watch_params);

This is a big problem. If my user is stuck in the device program after the upgrade, and they can only use it manually when they power on again. This is not good for our products. I hope Ti engineers can help solve this problem